:MEASure:CLOCk:DCDCycle:EDIRection
Command Syntax
:MEASure:CLOCk:DCDCycle:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:CLOCk:DCDCycle:EDIRection?
Description
For the Duty Cycle - Duty Cycle measurement, specifies the direction of the waveform's edges to be measured: rising or falling.
Example Command Sequence
This sequence sets up the measurement on rising edges only.
:MEASure:CLOCk:DCDCycle:SOURce CHAN1_1
:MEASure:CLOCk:DCDCycle:EDIRection RISing
// Perform measurement
:MEASure:CLOCk:DCDCycle
:MEASure:CLOCk:DCDCycle?