:MEASure:EYE:DCDistortion:FORMat

Command Syntax

:MEASure:EYE:DCDistortion:FORMat  {TIME | PERCent}

Query Syntax

:MEASure:EYE:DCDistortion:FORMat?

Description

Sets the format of the :DCDistortion measurement to either time or percent. Set the format before turning the measurement on.

Example Command Sequence

:MEASure:EYE:DCDistortion:SOURce ECHannel1
:MEASure:EYE:DCDistortion:FORMat TIME
:MEASure:EYE:DCDistortion
:MEASure:EYE:DCDistortion?