:MEASure:EYE:PAM:EHEight:DEFine:EOPening

Command Syntax

:MEASure:EYE:PAM:EHEight:DEFine:EOPening {ZHITs | PROBability}

Query Syntax

:MEASure:EYE:PAM:EHEight:DEFine:EOPening?

Description

Selects the method used to determine the eye-opening: zero hits (ZHITs) or probability (PROBabilitly). If probability is selected, use the :MEASure:EYE:PAM:EHEight:DEFine:EOPening:PROBability child command to enter the probability. The entered measurement-hit probability establishes the contour of an eye's opening. The default value is 1 x 10–18.