:MEASure:EYE:PAM:EHEight:STATus?
Query Syntax
:MEASure:EYE:PAM:EHEight:STATus?
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the :MEASure:EYE:PAM:EHEight measurement for PAM or NRZ signals. Use the :MEASure:EYE:PAM:EHEight:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:EYE:PAM:EHEight:STATus:DETails? child query.