:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:PROBability
Command Syntax
:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:PROBability <probability>
<probability> is a double.
Query Syntax
:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:PROBability?
Description
Sets the eye-opening probability for the Eye Widths measurement. The entered measurement-hit probability establishes the contour of an eye's opening. The probability can be set from 1 x 10–1 to 1 x 10–9. The default probability is 1 x 10–2. No extrapolation is used to determine Eye Widths at a specified probability. To select to use a probability target instead of zero data hits, use the :MEASure:EYE:PAM:EWIDth:DEFine:EOPening parent command.