:MEASure:EYE:PAM:EWIDth:LOCation?

Query Syntax

:MEASure:EYE:PAM:EWIDth:LOCation?

Description

Returns an location index of the :MEASure:EYE:PAM:EWIDth measurement for PAM or NRZ signals in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.