:MEASure:EYE:PAM:PP:LEVel
Command Syntax
:MEASure:EYE:PAM:PP:LEVel {LEVel0 | LEVel1 | LEVel2 | LEVel3}
Query Syntax
:MEASure:EYE:PAM:PP:LEVel?
Description
Selects the eye diagram's level on which to perform the :MEASure:EYE:PAM:PP measurement. The LEVel2 argument applies to PAM3 and PAM4 signals. The LEVel3 argument applies only to PAM4 signals. If you experience difficulties measuring a PAM signal, confirm that the signal-type setting is set appropriately using the :CHANnel:SIGNal:TYPE command.