:MEASure:EYE:PAM:PP:STATus:DETails?

Query Syntax

:MEASure:EYE:PAM:PP:STATus:DETails?

Description

Returns a string that may provide additional details for a failed :MEASure:EYE:PAM:PP measurement. If the measurement was successful, a null string is returned.

For a basic description of a measurement failure, use the :MEASure:EYE:PAM:PP:STATus:REASon? sibling query. Use the :MEASure:EYE:PAM:PP:STATus? parent query to determine if the measurement has failed.

See Also