:MEASure:EYE:WINDow:METHod

Command Syntax

:MEASure:EYE:WINDow:METHod {EOPening | CLOCk}

Query Syntax

:MEASure:EYE:WINDow:METHod?

Description

This command specifies how the eye window used for measurements is determined:

  • EOPening — Measures within an eye window defined by left and right opening locations.

    Use the :MEASure:EYE:WINDow:LEFT and :MEASure:EYE:WINDow:RIGHt commands to specify the left and right opening location values. The default values are 40% (left) and 60% (right) which identifies the central 20% of symbol period.

  • CLOCk — Measures within an eye window that is a width percentage at the location of the recovered clock edge.

    Use the :MEASure:EYE:WINDow:WIDTh command to specify the width percentage value.

This command is equivalent to the settings in the Eye tab of the Configure Measurements dialog box.