:MEASure:EYE:WINDow:WIDTh

Command Syntax

:MEASure:EYE:WINDow:WIDTh<percent>

<percent> is a double.

Query Syntax

:MEASure:EYE:WINDow:WIDTh?

Description

When the "At Clock Time" eye window determination method is selected (see :MEASure:EYE:WINDow:METHod), this command specifies the UI percentage width about the recovered clock location to use as the eye window. A zero percent for this setting means only the recovered clock location is used.

This command is equivalent to the settings in the Eye tab of the Configure Measurements dialog box.