:MEASure:FFT:FFRequency:FPLevel
Command Syntax
:MEASure:FFT:FFRequency:FPLevel <dBm>
<dBm> is a double.
Query Syntax
:MEASure:FFT:FFRequency:FPLevel?
Description
Defines the threshold an FFT peak must cross to be considered a peak in the FFT Frequency measurement (:MEASure:FFT:FFRequency). The default Peak Level is -40 dBm.