:MEASure:FFT:FFRequency:SOURce

Command Syntax

:MEASure:FFT:FFRequency:SOURce {FUNCtionN}

Where N identifies one of sixty four {1:64} FFT math functions that you can create. For example, FUNCtion3. To create a FFT function waveform, see :FUNCtion:FOPerator.

Query Syntax

:MEASure:FFT:FFRequency:SOURce?

Description

Selects the source FFT function waveform on which to perform the :MEASure:FFT:FFRequency measurement.