:MEASure:HORizontal:DCYCle

Command Syntax

:MEASure:HORizontal:DCYCle

Query Syntax

:MEASure:HORizontal:DCYCle?

Description

Performs a duty cycle measurement on NRZ waveforms. Moves the duty cycle measurement, which is the ratio of the positive pulse width to the period to the top of the Results table. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value. Sources can be any displayed waveform, waveform memory, or function. For example, CHAN1_1, WMEMory1, or FUNCtion1.

Example Command Sequence

:MEASure:HORizontal:DCYCle:SOURce CHAN2_1
:MEASure:HORizontal:DCYCle:EDIRection RISing
:MEASure:HORizontal:DCYCle
:MEASure:HORizontal:DCYCle?

Measurement Ready?

To confirm that the measurement is ready to read, you can query the measurement's status:

if ('CORR' in Infiniium.query(':MEASure:HORizontal:DCYCle:STATus?')):
	measurement = Infiniium.query(':MEASure:HORizontal:DCYCle?')

If averaging is turned on (:ACQuire:SMODe AVERage), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:COUNt?) versus the number of measurement sweeps that have occurred (:ACQuire:COUNt?). The technique uses the :COUNt? common measurement query. For example,

if (Infiniium.query(':MEASure:HORizontal:DCYCle:COUNt?') >= Infiniium.query(':ACQuire:COUNt?')):
	measurement = Infiniium.query(':MEASure:HORizontal:DCYCle?')

You can also use an acquisition limit test to test that a number of waveforms or samples have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.

Querying Measurement Results and Statistics

You can query measurement results using the :MEASure:HORizontal:DCYCle? query after making the proper instance settings.

If a measurement is installed into Results table (using the :MEASure:HORizontal:DCYCle command) and you have made the proper instance settings, you can query statistics using common child queries.

Also, you can query measurement results and statistics directly from the Results table (without having to make the proper instance settings beforehand). See Querying Measurement Results and Statistics.