:MEASure:HORizontal:DCYCle:EDIRection
Command Syntax
:MEASure:HORizontal:DCYCle:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:HORizontal:DCYCle:EDIRection?
Description
For the duty cycle measurement, specifies the edge on which to start the measurement.
RISing— the cycle(s) on which the measurement is made begin with a rising edge.FALLing— the cycle(s) on which the measurement is made begin with a falling edge.