:MEASure:HORizontal:FREQuency:EDIRection

Command Syntax

:MEASure:HORizontal:FREQuency:EDIRection  {RISing | FALLing}

Query Syntax

:MEASure:HORizontal:FREQuency:EDIRection?

Description

Specifies whether the frequency measurement is made from rising edge to rising edge or falling edge to falling edge.

  • RISing — the cycle(s) on which the measurement is made begin with a rising edge.
  • FALLing — the cycle(s) on which the measurement is made begin with a falling edge.

To set the edge threshold, use the Threshold Configuration Commands.