Threshold Configuration Commands

The following commands let you specify global thresholds and top-base definitions:

The following commands let you specify thresholds and top-base definitions for individual waveforms:

Waveform threshold levels can be set to standard percentages or to custom user definitions based on absolute amplitudes.

Threshold levels definitions affect the measurements listed in the following table.

Measurements Affected by Threshold Levels Definitions
Oscilloscope
Mode
Eye/Mask
Mode
Average Duty Cycle Distortion
Duty Cycle Rise Time
Fall Time Fall Time
Frequency  
Preshoot  
Overshoot  
Period  
Pulse Width  
Rise Time  
Δ Time  
Time at Edge  
Time at Amplitude  
RMS  
Amplitude at Lower  
Amplitude at Middle  
Amplitude at Lower  
Optical Modulation Amplitude  
Jitter