:MEASure:HORizontal:FTIMe:STATus:REASon?

Query Syntax

:MEASure:HORizontal:FTIMe:STATus:REASon?

Description

Returns a string that explains the reason for a failed :MEASure:HORizontal:FTIMe measurement. If the measurement was successful, a null string is returned.

Additional information about the failure may be available using the :MEASure:HORizontal:FTIMe:STATus:DETails? sibling query. Use the :MEASure:HORizontal:FTIMe:STATus? parent query to determine if the measurement has failed.

See Also