:MEASure:HORizontal:FTIMe:UREFerence:STATe
Command Syntax
:MEASure:HORizontal:FTIMe:UREFerence:STATe {ON | OFF | 1 | 0}
Query Syntax
:MEASure:HORizontal:FTIMe:UREFerence:STATe?
Query Response
{1 | 0}
Description
Enables or disables a user-defined horizontal reference location near which a one-measurement-per-acquisition measurement is made.
When a user-defined horizontal reference location is enabled, the :MEASure:HORizontal:FTIMe:UREFerence:VALue command specifies its time location with respect to the trigger (t = 0) location.