:MEASure:HORizontal:HTIMe:DEDirection

Command Syntax

:MEASure:HORizontal:HTIMe:DEDirection {RISing | FALLing | BOTH}

Query Syntax

:MEASure:HORizontal:HTIMe:DEDirection?

Description

For the :MEASure:HORizontal:HTIMe measurement, specifies which data signal edges to include in the measurement.

The BOTH option means both rising and falling data signal edges are included in the measurement.

Example Command Sequence

This sequence sets up the measurement using both data signal edges and the falling clock signal edge.

:MEASure:HORizontal:HTIMe:SOURce1 CHAN1_1
:MEASure:HORizontal:HTIMe:SOURce2 CHAN1_2
:MEASure:HORizontal:HTIMe:DEDirection BOTH
:MEASure:HORizontal:HTIMe:CEDirection FALLing
//  Perform measurement
:MEASure:HORizontal:HTIMe
:MEASure:HORizontal:HTIMe?