:MEASure:HORizontal:HTIMe:OCCurrences

Command Syntax

:MEASure:HORizontal:HTIMe:OCCurrences  ALL

Query Syntax

:MEASure:HORizontal:HTIMe:OCCurrences?

Description

This command has only the ALL option because the measurement makes multiple measurements per acquisition using all edges in the acquisition only (and has no option for making one measurement per acquisition).

The "Current" measurement result (see :MEASure:RESults?) is taken from the measurement closest to the timebase reference. For measurements on memory waveforms, the "Current" measurement is the one closest to the horizontal X position setting. Annotations are shown at the "Current" measurement result.