:MEASure:HORizontal:NPERiod:EDIRection

Command Syntax

:MEASure:HORizontal:NPERiod:EDIRection {RISing | FALLing}

Query Syntax

:MEASure:HORizontal:NPERiod:EDIRection?

Description

For the :MEASure:HORizontal:NPERiod measurement, specifies which signal edges to include in the measurement.

Example Command Sequence

This sequence sets up the measurement using rising signal edges and 10 periods.

:MEASure:HORizontal:NPERiod:SOURce CHAN1_1
:MEASure:HORizontal:NPERiod:EDIRection RISing
:MEASure:HORizontal:NPERiod:NPERiods 10
//  Perform measurement
:MEASure:HORizontal:NPERiod
:MEASure:HORizontal:NPERiod?