:MEASure:HORizontal:NPERiod:NPERiods

Command Syntax

:MEASure:HORizontal:NPERiod:NPERiods <number_of_periods>
            

<number_of_periods> is an integer.

Query Syntax

:MEASure:HORizontal:NPERiod:NPERiods?

Description

For the :MEASure:HORizontal:NPERiod measurement, specifies the number of periods to include in the measurement.

Example Command Sequence

This sequence sets up the measurement using rising signal edges and 10 periods.

:MEASure:HORizontal:NPERiod:SOURce CHAN1_1
:MEASure:HORizontal:NPERiod:EDIRection RISing
:MEASure:HORizontal:NPERiod:NPERiods 10
//  Perform measurement
:MEASure:HORizontal:NPERiod
:MEASure:HORizontal:NPERiod?