:MEASure:HORizontal:PERiod:EDIRection
Command Syntax
:MEASure:HORizontal:PERiod:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:HORizontal:PERiod:EDIRection?
Description
Specifies whether the period measurement is made from rising edge to rising edge or falling edge to falling edge.
RISing— the cycle(s) on which the measurement is made begin with a rising edge.FALLing— the cycle(s) on which the measurement is made begin with a falling edge.
To set the edge threshold, use the Threshold Configuration Commands.