:MEASure:HORizontal:PHASe:EDIRection

Command Syntax

:MEASure:HORizontal:PHASe:EDIRection{1:2}  {RISing | FALLing}

Query Syntax

:MEASure:HORizontal:PHASe:EDIRection?

Description

For the phase measurement, specifies the waveform's edge direction used to identify the first or second measurement edge: rising or falling.

To set the edge threshold, use the Threshold Configuration Commands.

Example Command Sequence

This sequence defines source one's edge number, direction, and threshold followed by source two's edge number, direction, and threshold. The delta time measurement is then started and the measurement result returned.

:MEASure:HORizontal:PHASe:SOURce1 CHAN1_1
//  Defines first measurement edge
:MEASure:HORizontal:PHASe:EDIRection1 RISing
//  Defines second measurement edge
:MEASure:HORizontal:PHASe:SOURce2 WMEMory1
:MEASure:HORizontal:PHASe:EDIRection2 FALLing
//  Perform measurement
:MEASure:HORizontal:PHASe
:MEASure:HORizontal:PHASe?