:MEASure:HORizontal:SLEWrate:EDIRection
Command Syntax
:MEASure:HORizontal:SLEWrate:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:HORizontal:SLEWrate:EDIRection?
Description
For the slew rate measurement, specifies the waveform's edges to be measured: rising or falling edges.
Example Command Sequence
This sequence sets up the measurement on rising edges only.
:MEASure:HORizontal:SLEWrate:SOURce CHAN1_1
:MEASure:HORizontal:SLEWrate:EDIRection RISing
// Perform measurement
:MEASure:HORizontal:SLEWrate
:MEASure:HORizontal:SLEWrate?