:MEASure:HORizontal:SLEWrate:SOURce
Command Syntax
:MEASure:HORizontal:SLEWrate:SOURce {CHANnel{N} | DIFF{1:8}{A|C} | FUNCtion{1:64} | WMEMory{1:8}}
{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:MEASure:HORizontal:SLEWrate:SOURce?
Description
Selects the source waveform on which to perform the :MEASure:HORizontal:SLEWrate measurement.