:MEASure:JITTer:JITTer:ISI:STATus:DETails?
Query Syntax
:MEASure:JITTerN:JITTer:ISI:STATus:DETails?
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Description
Returns a string that may provide additional details for a failed :MEASure:JITTer:JITTer:ISI? measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :MEASure:JITTer:JITTer:ISI:STATus:REASon? sibling query. Use the :MEASure:JITTer:JITTer:ISI:STATus? parent query to determine if the measurement has failed.