:MEASure:JITTer:NOISe:EHEight:EYE
Command Syntax
:MEASure:JITTerN:NOISe:EHEight:EYE {EYE0}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:NOISe:EHEight:EYE?
Description
This command specifies the eye for which the measurement value is returned. With NRZ signals, there is one eye only, EYE0.