:MEASure:JITTer:NOISe:EHEight:STATus:DETails?

Query Syntax

:MEASure:JITTerN:NOISe:EHEight:STATus:DETails?

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Description

Returns a string that may provide additional details for a failed :MEASure:JITTer:NOISe:EHEight? measurement. If the measurement was successful, a null string is returned.

For a basic description of a measurement failure, use the :MEASure:JITTer:NOISe:EHEight:STATus:REASon? sibling query. Use the :MEASure:JITTer:NOISe:EHEight:STATus? parent query to determine if the measurement has failed.

See Also