:MEASure:JITTer:NOISe:GRAPh:ISISymbol
Command Syntax
:MEASure:JITTerN:NOISe:GRAPh:ISISymbol {ON | OFF | 1 | 0}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:NOISe:GRAPh:ISISymbol?
Query Response
{1 | 0}
Description
Enables or disables the ISI vs Symbol noise graph.