:MEASure:JITTer:NOISe:MGRaph
Command Syntax
:MEASure:JITTerN:NOISe:MGRaph {NSPectrum | RNPihist | TIHist | ISIHist | ABAThtub
| ISISymbol | IFILter | CTIHist | SLEVels | PATTern}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:NOISe:MGRaph?
Description
This command selects the Jitter graph that should be maximized in the graph display area when using the :MEASure:JITTer:NOISe:DMAXimized command:
NSPectrum— Noise SpectrumRNPihist— RN/PI HistogramTIHist— TI HistogramISIHist— ISI HistogramABAThtub— Noise BathtubISISymbol— ISI vs SymbolIFILter— ISI FilterCTIHist— Composite TI HistogramSLEVels— ???PATTern— ???