:MEASure:JITTer:NOISe:ISI?
Query Syntax
:MEASure:JITTerN:NOISe:ISI?
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Description
Returns ISI (p-p), Inter-Symbol Interference, which is a measure of the pattern-dependent interference effects within a signal. It is a measure of how much the amplitude of a bit depends on its location within the pattern. The value is returned for the level specified by :MEASure:JITTer:NOISe:ISI:LEVel.