:MEASure:JITTer:NOISe:ISI:STATus?
Query Syntax
:MEASure:JITTerN:NOISe:ISI:STATus?
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid.
- QUES
- The measurement result is questionable.
Description
Queries the status of the :MEASure:JITTer:NOISe:ISI? measurement. Use the :MEASure:JITTer:NOISe:ISI:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:JITTer:NOISe:ISI:STATus:DETails? child query.