:MEASure:JITTer:NOISe:VECLosure:EYE
Command Syntax
:MEASure:JITTerN:NOISe:VECLosure:EYE {EYE0}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:NOISe:VECLosure:EYE?
Description
This command specifies the eye for which the measurement value is returned. Multiple eyes are present in PAM signals.