:MEASure:LLINe:LINE:MLOCation?
Query Syntax
:MEASure:LLINeN:LINEM:MLOCation?
Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.
Where M identifies one of 16 {1:16} possible limit lines.
Description
Queries the location in time of the data point where the pass/fail margin is reported for a specific limit line. The returned time value is the same value that is shown in the Details dialog box which is displayed from the Limit Lines panel. To return the pass/fail margin, use the :MEASure:LLINe:LINE:MARGin? query. To return the total number of failed data points (which is zero for positive margins) use the :MEASure:LLINe:LINE:FPOints? query. To load and display a Limit Line Test, use the :LLINe:DISPlay command.
Only displayed data points are analyzed. For example, if you zoom in on the waveform so that a portion of the Limit Line Test is off screen, any failed data point that exists off screen will not be analyzed.