:MEASure:LLINe:MLOCation:STATus?

Query Syntax

:MEASure:LLINeN:MLOCation:STATus?

Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid.
QUES
The measurement result is questionable.

Description

Queries the status of the :MEASure:LLINe:MLOCation? measurement. Use the :MEASure:LLINe:MLOCation:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. .

See Also