:MEASure:LLINe:MLOCation?
Query Syntax
:MEASure:LLINeN:MLOCation?
Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.
Description
Queries the location in time of the data point where the pass/fail margin is reported for a Limit Line Test. The returned time value is the same value that is shown in the displayed Limit Lines panel. To return the pass/fail margin, use the :MEASure:LLINe:MARGin? query. To return the total number of failed data points for the Limit Line Test, use the :MEASure:LLINe:FPOints? query. To load and display a Limit Line Test, use the :LLINe:DISPlay command.
Only displayed data points are analyzed. For example, if you zoom in on the waveform so that a portion of the Limit Line Test is off screen, any failed data point that exists off screen will not be analyzed.