:MEASure:LLINe:MARGin:STATus?
Query Syntax
:MEASure:LLINeN:MARGin:STATus?
Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid.
- QUES
- The measurement result is questionable.
Description
Queries the status of the :MEASure:LLINe:MARGin? measurement for a Limit Line Test. Use the :MEASure:LLINe:MARGin:STATus:REASon? child query to determine the reason for an invalid or questionable measurement.