:MEASure:LLINe:MARGin:STATus:REASon?

Query Syntax

:MEASure:LLINeN:MARGin:STATus:REASon?

Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed :MEASure:LLINe:MARGin? measurement. If the measurement was successful, a null string is returned. Use the :MEASure:LLINe:MARGin:STATus? parent query to determine if the measurement has failed.

See Also