:MEASure:MARKer:DY?

Query Syntax

:MEASure:MARKer:DY{1:4}{A:C}?

This command supports the STATus? and STATus:REASon?common child commands.

Description

Queries the difference in time between any two Y-axis markers, whether they are tracking marker pair or manual line markers. The two markers can have different source waveforms. Use the :MARKer subsystem to turn on markers. To display or hide the Δ Position and Δ Magnitude listings in the displayed Markers table, use the :DISPlay:MARKer:DELTas command.

Example Command Sequence

:MARKer:Y1A:SOURce CHANnel1
:MARKer:Y2A:SOURce CHANnel2
:MARKer:Y1A:STATe MANual//  Marker 1 turned on as a manual line marker
:MARKer:Y2A:STATe TRAC//  Marker 2 turned on as a  tracking marker pair
…
:MEASure:MARKer:DY2A?