:MEASure:MARKer:DY:STATus?

Query Syntax

:MEASure:MARKer:DY{1:4}{A:C}:STATus?

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid.
QUES
The measurement result is questionable.

Description

Queries the status of the DY? measurement. Use the STATus:REASon? child query to determine the reason for a invalid or questionable measurement.

See Also