:MEASure:MARKer:IDX:STATus:REASon?

Query Syntax

:MEASure:MARKer:IDX:STATus:REASon?

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed IXDelta measurement. If the measurement was successful, a null string is returned. Use the STATus? query to determine if the measurement has failed.

See Also