:MEASure:MARKer:IDX?

Query Syntax

:MEASure:MARKer:IDX{1:4}?

This command supports the STATus? and STATus:REASon?common child commands.

Description

Queries the reciprocal of the DX? marker measurement. The two markers can have different source waveforms. Use the :MARKer subsystem to turn on markers.

Example Command Sequence

:MARKer:X1:SOURce CHANnel1
:MARKer:X2:SOURce CHANnel2
:MARKer:Y1A:STATe TRAC  //  Marker 1 turned on as a manual marker
:MARKer:Y2A:STATe TRAC  //  Marker 2 turned on as a waveform tracking marker
…
:MEASure:MARKer:IDX2?