:MEASure:MARKer:Y?

Query Syntax

:MEASure:MARKer:Y{1:4}{A:C}?

This command supports the STATus? and STATus:REASon? common child commands.

Description

This command queries the amplitude of a Y-axis manual-line marker or tracking marker pair.

With S-parameter magnitude, phase, and group delay waveforms displayed, you can create one tracking marker at an X value that has three different Y values, one from each waveform at the same X value. In other words, this single tracking marker has three Y values at the same X position. All three Y values are shown in additional Magnitude columns in the marker results table. The following table shows how to identify the Y values in the query. Each waveform is identified using a letter from A to C.

Example of Querying S-Parameter Y Marker Values
Y Value Example Marker 2 Query
Magnitude Y Value :MEASure:MARKer:Y2A?
Phase Y Value :MEASure:MARKer:Y2B?
Group Delay Y Value :MEASure:MARKer:Y2C?

To turn on a marker, use the commands in the :MARKer subsystem.

Example Command Sequence

:MARKer:Y1A:SOURce CHANnel1
:MARKer:Y1A:STATe TRACking
…
:MEASure:MARKer:Y1A?