:MEASure:MARKer:Y:STATus:REASon?

Query Syntax

:MEASure:MARKer:Y{1:4}{A:C}:STATus:REASon?

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed Y measurement. If the measurement was successful, a null string is returned. Use the STATus? query to determine if the measurement has failed.

See Also