:MEASure:MTESt:FUINtervals:STATus?

Query Syntax

:MEASure:MTESt{N}:FUINtervals:STATus?

{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid.
QUES
The measurement result is questionable.

Description

Queries the status of the FUINtervals measurement. Use the :MEASure:MTESt:FUINtervals:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:MTESt:FUINtervals:STATus:DETails? child query.

See Also