:MEASure:MTESt:HREGion{N}?
Query Syntax
:MEASure:MTESt{N}:HREGion{1:16}?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Description
Returns the number of violations for a standard mask Region reported in the Masks Tests results table during eye mask testing. Include the region's identification number, as displayed on the mask, in the command. For example, to query the violations for Region 2, use this query:
:MEASure:MTESt{N}:HREGion2?
If a positive mask margin is applied, this count does not include any point within the region's margin area. If a negative mask margin is applied, this count does include points within the region's margin area.
If the selected region is defined by the mask, this command returns an integer (number of violations) and the :STATus? child query returns CORR. If the region is not defined by the mask, this command returns "9.91E+37 (NaN)", the :STATus? child query returns INV, and the :STATus:REASon? child query returns the string "Invalid Region".
To query the total number of violations for all mask regions, use the :MEASure:MTESt:HITS? command.