:MEASure:MTESt:HITS?
Query Syntax
:MEASure:MTESt{N}:HITS?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Description
Returns the number of Total Standard Mask Violations reported in the Masks Tests results table during eye mask testing. For positive margins, this count does not include any point within the margin area. For negative margins, this count does include points within the margin area. To query the number of violations for a specific mask region (as labeled on the display), use the :MEASure:MTESt:HREGion{N}? command.