:MEASure:MTESt:MHITs?

Query Syntax

:MEASure:MTESt{N}:MHITs?

{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.

Description

Returns the number of Total Margin Mask Violations reported in the Masks Tests results table during eye mask testing. For positive margins, this count does include any point within the standard mask area. For negative margins, this count only includes points within the margin but not outside the margin area into the standard mask area. To query the number of violations for a margin area associated with a specific mask region (as labeled on the display), use the :MEASure:MTESt:MHRegion{N}? command.