:MEASure:MTESt:MHRegion{N}:STATus?
Query Syntax
:MEASure:MTESt{N}:MHRegion{1:16}:STATus?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid.
- QUES
- The measurement result is questionable.
Description
Queries the status of the MHRegion measurement. Use the :MEASure:MTESt:MHRegion{N}:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:MTESt:MHRegion:STATus:DETails? child query.